Hexiwear Sample codes without RTOS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hexiwear Sample codes without RTOS

1,268件の閲覧回数
aravindapn
Contributor I

We have obtained a Hexiwear device and would like to customize the code to use only few of the sensors(MAXIM), display and the BLE. We do not need the menus and the navigation using the keys. I looked into the example code "MK64" and understand that it uses a RTOS and scheduling mechanism to handle the various user inputs/navigations, etc. How do we adapt this code so that we get rid of the user input and cause the device to automatically start reading the MAXIM sensor data, for instance.

Are there any other example codes that do not use the scheduler but just perform basic sensor read and transmit through BLE. It would be helpful if you could share such KDS workspaces if they are available.

Please suggest.

Thanks,

Aravinda

タグ(1)
0 件の賞賛
返信
0 返答(返信)