Kinetis K22F reference manual link broken

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis K22F reference manual link broken

1,979 Views
asfarley
Contributor IV

Hi,

I'm trying to download the K22F reference manual from the NXP site but I keep getting a broken link. This happens on both Chrome and Firefox so I don't think it's just the browser.

Labels (1)
0 Kudos
Reply
3 Replies

1,899 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Alexander,

I've checked the links for both reference manuals and at the moment they are working:

Here is the one for 256KB Flash:

https://www.nxp.com/webapp/Download?colCode=K22P121M120SF8RM 

Here is the one for 512KB Flash:

https://www.nxp.com/webapp/Download?colCode=K22P121M120SF7RM 

Hope this helps!

Have a great day!

Sabina

0 Kudos
Reply

1,899 Views
mjbcswitzerland
Specialist V

Hi

I can also confirm that they are working today.

Regards

Mark

0 Kudos
Reply

1,899 Views
mjbcswitzerland
Specialist V

Alexander

There is presently a problem on the web site.

I have a attached a selection of K22 reference manuals (there are in fact about 10 different ones available, depending on exact part) to keep you going until it is fixed.

Regards

Mark

0 Kudos
Reply