Kinetis Flash Technology

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Flash Technology

Jump to solution
1,993 Views
stefaneisenreic
Contributor I

Hi

I am wondering which flash technology is implemented inside the Kinetis Kx MCUs, NAND or NOR flash technology?

Thanks!

Regards

0 Kudos
Reply
1 Solution
1,834 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Stefan,

The kind of flash inside the Kientis is the NOR Flash.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,835 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Stefan,

The kind of flash inside the Kientis is the NOR Flash.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,834 Views
stefaneisenreic
Contributor I

Hi, Thanks!!

0 Kudos
Reply