Kinetis E microcontroller support in SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis E microcontroller support in SDK

1,971 Views
ChrisDarrow
Contributor III


Hello NXP,

Do you intend to add Kinetis E micro support in the SDK going forward?

Thanks,
Chris

Labels (1)
0 Kudos
Reply
2 Replies

1,689 Views
DavidS
NXP Employee
NXP Employee

To add to Jorge's statement:

A NXP FAE ported it to KDS and here that is.

Here’s the link to the updated FRDM-KEXX Driver Library Package driver with KDS support for all the example projects

  https://community.freescale.com/docs/DOC-329476

Regards,

David

0 Kudos
Reply

1,689 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Chris Darrow:

Thank you for using our community.

Unfortunately there are currently no plans to add Kinetis E support in KSDK.

For this family NXP has the next software options:

1) Processor Expert drivers: Processor Expert is integrated with Kinetis_Design_Studio. Processor Expert projects generated in KDS can be also used with IAR or Keil:

https://mcuoneclipse.com/2015/06/28/tutorial-using-kinetis-design-studio-v3-0-0-with-iar-and-keil-id...

2) There is a package with baremetal drivers in the next page under "Downloads -> Device Drivers":

Freedom Development Platform for Kinetis KE02|NXP


Best regards,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply