Kinetis Controller Not Replying Properly in SPI Slave Mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kinetis Controller Not Replying Properly in SPI Slave Mode

跳至解决方案
2,012 次查看
waqasbutt
Contributor II

Hello,

I am using K20 series controller. In slave mode the controller keeps sending the first value that has been pushed through PUSHR_SLAVE. It never updates.

The slave is receiving data correctly which can be seen through the oscilloscope. The settings CPHA and CPOL also match in slave and master

Images of Oscilloscope

1. Yellow (Clk)

2. Blue    (Slave Out)

3. Purple (Master Out)

4. Green (Chip Select)

DS0001.PNG

DS0002.PNG

Slave Code is as follows

SLAVE:

// Initialization
void SPI1_Init(void)
{
 /* SIM_SCGC6: DSPI1=1 */
 SIM_SCGC6 |= SIM_SCGC6_DSPI1_MASK;
 /* SPI1_MCR: MSTR=0,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=0,??=0,??=0,PCSIS=0,DOZE=0,MDIS=0,DIS_TXF=0,DIS_RXF=0,CLR_TXF=0,CLR_RXF=0,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */
 SPI1_MCR = SPI_MCR_DCONF(0x00) |
 SPI_MCR_PCSIS(0x00) |
 SPI_MCR_SMPL_PT(0x00) |
 SPI_MCR_HALT_MASK;
 /* SPI1_MCR: MSTR=0,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=0,??=0,??=0,PCSIS=0x0F,DOZE=0,MDIS=0,DIS_TXF=1,DIS_RXF=1,CLR_TXF=1,CLR_RXF=1,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */
 SPI1_MCR = SPI_MCR_DCONF(0x00) |
 SPI_MCR_PCSIS(0x0F) |
 SPI_MCR_DIS_TXF_MASK |
 SPI_MCR_DIS_RXF_MASK |
 SPI_MCR_CLR_TXF_MASK |
 SPI_MCR_CLR_RXF_MASK |
 SPI_MCR_SMPL_PT(0x00) |
 SPI_MCR_HALT_MASK;
 /* SPI1_TCR: SPI_TCNT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
 SPI1_TCR = SPI_TCR_SPI_TCNT(0x00);
 /* SPI1_CTAR1: DBR=0,FMSZ=0x0F,CPOL=0,CPHA=0,LSBFE=0,PCSSCK=0,PASC=0,PDT=0,PBR=0,CSSCK=0,ASC=0,DT=0,BR=0 */
 SPI1_CTAR1 = SPI_CTAR_FMSZ(0x0F) |
 SPI_CTAR_PCSSCK(0x00) |
 SPI_CTAR_PASC(0x00) |
 SPI_CTAR_PDT(0x00) |
 SPI_CTAR_PBR(0x00) |
 SPI_CTAR_CSSCK(0x00) |
 SPI_CTAR_ASC(0x00) |
 SPI_CTAR_DT(0x00) |
 SPI_CTAR_BR(0x00);
 /* SPI1_CTAR0_SLAVE: FMSZ=7,CPOL=0,CPHA=0 */
 SPI1_CTAR0_SLAVE = (uint32_t)((SPI1_CTAR0_SLAVE & (uint32_t)~(uint32_t)(
 SPI_CTAR_SLAVE_FMSZ(0x18) |
 SPI_CTAR_SLAVE_CPOL_MASK |
 SPI_CTAR_SLAVE_CPHA_MASK
 )) | (uint32_t)(
 SPI_CTAR_SLAVE_FMSZ(0x07)
 ));
 /* SPI1_SR: TCF=1,TXRXS=1,??=0,EOQF=1,TFUF=1,??=0,TFFF=1,??=0,??=0,??=0,??=0,??=0,RFOF=1,??=0,RFDF=1,??=0,TXCTR=0,TXNXTPTR=0,RXCTR=0,POPNXTPTR=0 */
 SPI1_SR = SPI_SR_TCF_MASK |
 SPI_SR_TXRXS_MASK |
 SPI_SR_EOQF_MASK |
 SPI_SR_TFUF_MASK |
 SPI_SR_TFFF_MASK |
 SPI_SR_RFOF_MASK |
 SPI_SR_RFDF_MASK |
 SPI_SR_TXCTR(0x00) |
 SPI_SR_TXNXTPTR(0x00) |
 SPI_SR_RXCTR(0x00) |
 SPI_SR_POPNXTPTR(0x00);
 /* SPI1_RSER: TCF_RE=0,??=0,??=0,EOQF_RE=0,TFUF_RE=0,??=0,TFFF_RE=0,TFFF_DIRS=0,??=0,??=0,??=0,??=0,RFOF_RE=0,??=0,RFDF_RE=1,RFDF_DIRS=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
 SPI1_RSER = SPI_RSER_RFDF_RE_MASK;
 /* SPI1_MCR: HALT=0 */
 SPI1_MCR &= (uint32_t)~(uint32_t)(SPI_MCR_HALT_MASK);
}


// Service Routine
PE_ISR(INT_SPI1_HANDLER)
{
    uint32_t receivedValue = SPI1_POPR;
    uint8_t valueToSend = 0;

   SPI1_SR = SPI_SR_RFDF_MASK | SPI_SR_TCF_MASK;
    if(receivedValue == 0x81)
       valueToSend = 0xF0;
    else
       valueToSend = 0x0F;
   while((SPI1_SR & SPI_SR_TFFF_MASK)==0);
   SPI1_PUSHR_SLAVE = valueToSend;
}
0 项奖励
回复
1 解答
1,823 次查看
waqasbutt
Contributor II

Problem solved.

It was a hardware problem. cs pin was not correctly attached

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,824 次查看
waqasbutt
Contributor II

Problem solved.

It was a hardware problem. cs pin was not correctly attached

0 项奖励
回复