Kinetis Controller Not Replying Properly in SPI Slave Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Controller Not Replying Properly in SPI Slave Mode

Jump to solution
2,016 Views
waqasbutt
Contributor II

Hello,

I am using K20 series controller. In slave mode the controller keeps sending the first value that has been pushed through PUSHR_SLAVE. It never updates.

The slave is receiving data correctly which can be seen through the oscilloscope. The settings CPHA and CPOL also match in slave and master

Images of Oscilloscope

1. Yellow (Clk)

2. Blue    (Slave Out)

3. Purple (Master Out)

4. Green (Chip Select)

DS0001.PNG

DS0002.PNG

Slave Code is as follows

SLAVE:

// Initialization
void SPI1_Init(void)
{
 /* SIM_SCGC6: DSPI1=1 */
 SIM_SCGC6 |= SIM_SCGC6_DSPI1_MASK;
 /* SPI1_MCR: MSTR=0,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=0,??=0,??=0,PCSIS=0,DOZE=0,MDIS=0,DIS_TXF=0,DIS_RXF=0,CLR_TXF=0,CLR_RXF=0,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */
 SPI1_MCR = SPI_MCR_DCONF(0x00) |
 SPI_MCR_PCSIS(0x00) |
 SPI_MCR_SMPL_PT(0x00) |
 SPI_MCR_HALT_MASK;
 /* SPI1_MCR: MSTR=0,CONT_SCKE=0,DCONF=0,FRZ=0,MTFE=0,PCSSE=0,ROOE=0,??=0,??=0,PCSIS=0x0F,DOZE=0,MDIS=0,DIS_TXF=1,DIS_RXF=1,CLR_TXF=1,CLR_RXF=1,SMPL_PT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,HALT=1 */
 SPI1_MCR = SPI_MCR_DCONF(0x00) |
 SPI_MCR_PCSIS(0x0F) |
 SPI_MCR_DIS_TXF_MASK |
 SPI_MCR_DIS_RXF_MASK |
 SPI_MCR_CLR_TXF_MASK |
 SPI_MCR_CLR_RXF_MASK |
 SPI_MCR_SMPL_PT(0x00) |
 SPI_MCR_HALT_MASK;
 /* SPI1_TCR: SPI_TCNT=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
 SPI1_TCR = SPI_TCR_SPI_TCNT(0x00);
 /* SPI1_CTAR1: DBR=0,FMSZ=0x0F,CPOL=0,CPHA=0,LSBFE=0,PCSSCK=0,PASC=0,PDT=0,PBR=0,CSSCK=0,ASC=0,DT=0,BR=0 */
 SPI1_CTAR1 = SPI_CTAR_FMSZ(0x0F) |
 SPI_CTAR_PCSSCK(0x00) |
 SPI_CTAR_PASC(0x00) |
 SPI_CTAR_PDT(0x00) |
 SPI_CTAR_PBR(0x00) |
 SPI_CTAR_CSSCK(0x00) |
 SPI_CTAR_ASC(0x00) |
 SPI_CTAR_DT(0x00) |
 SPI_CTAR_BR(0x00);
 /* SPI1_CTAR0_SLAVE: FMSZ=7,CPOL=0,CPHA=0 */
 SPI1_CTAR0_SLAVE = (uint32_t)((SPI1_CTAR0_SLAVE & (uint32_t)~(uint32_t)(
 SPI_CTAR_SLAVE_FMSZ(0x18) |
 SPI_CTAR_SLAVE_CPOL_MASK |
 SPI_CTAR_SLAVE_CPHA_MASK
 )) | (uint32_t)(
 SPI_CTAR_SLAVE_FMSZ(0x07)
 ));
 /* SPI1_SR: TCF=1,TXRXS=1,??=0,EOQF=1,TFUF=1,??=0,TFFF=1,??=0,??=0,??=0,??=0,??=0,RFOF=1,??=0,RFDF=1,??=0,TXCTR=0,TXNXTPTR=0,RXCTR=0,POPNXTPTR=0 */
 SPI1_SR = SPI_SR_TCF_MASK |
 SPI_SR_TXRXS_MASK |
 SPI_SR_EOQF_MASK |
 SPI_SR_TFUF_MASK |
 SPI_SR_TFFF_MASK |
 SPI_SR_RFOF_MASK |
 SPI_SR_RFDF_MASK |
 SPI_SR_TXCTR(0x00) |
 SPI_SR_TXNXTPTR(0x00) |
 SPI_SR_RXCTR(0x00) |
 SPI_SR_POPNXTPTR(0x00);
 /* SPI1_RSER: TCF_RE=0,??=0,??=0,EOQF_RE=0,TFUF_RE=0,??=0,TFFF_RE=0,TFFF_DIRS=0,??=0,??=0,??=0,??=0,RFOF_RE=0,??=0,RFDF_RE=1,RFDF_DIRS=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0,??=0 */
 SPI1_RSER = SPI_RSER_RFDF_RE_MASK;
 /* SPI1_MCR: HALT=0 */
 SPI1_MCR &= (uint32_t)~(uint32_t)(SPI_MCR_HALT_MASK);
}


// Service Routine
PE_ISR(INT_SPI1_HANDLER)
{
    uint32_t receivedValue = SPI1_POPR;
    uint8_t valueToSend = 0;

   SPI1_SR = SPI_SR_RFDF_MASK | SPI_SR_TCF_MASK;
    if(receivedValue == 0x81)
       valueToSend = 0xF0;
    else
       valueToSend = 0x0F;
   while((SPI1_SR & SPI_SR_TFFF_MASK)==0);
   SPI1_PUSHR_SLAVE = valueToSend;
}
0 Kudos
Reply
1 Solution
1,827 Views
waqasbutt
Contributor II

Problem solved.

It was a hardware problem. cs pin was not correctly attached

View solution in original post

0 Kudos
Reply
1 Reply
1,828 Views
waqasbutt
Contributor II

Problem solved.

It was a hardware problem. cs pin was not correctly attached

0 Kudos
Reply