Kinetis Bootloader using SPI

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Kinetis Bootloader using SPI

跳至解决方案
3,018 次查看
motisonnenfeld
Contributor I

Hi all,

I am trying to use the Kinetis ROM Bootloader via SPI but don't seem to find the pin muxing anywhere in the documentation

I have a FRDM-KL03Z which has a single SPI module but its signals can be muxed to several pin combinations (none of which is the default pin function)

Thanks,

Moti

标记 (3)
0 项奖励
回复
1 解答
2,257 次查看
adriancano
NXP Employee
NXP Employee

Hi,

In the KL03 reference manual under the Chapter 11 Kinetis ROM Bootloader you can fin the Kinetis Bootloader Peripheral Pinmux that lists the PTA6 and PTA7 as the SPI pins for the Kinetis Bootloader.

kboot kl03.png
Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,258 次查看
adriancano
NXP Employee
NXP Employee

Hi,

In the KL03 reference manual under the Chapter 11 Kinetis ROM Bootloader you can fin the Kinetis Bootloader Peripheral Pinmux that lists the PTA6 and PTA7 as the SPI pins for the Kinetis Bootloader.

kboot kl03.png
Hope this information can help you

Best Regards,
Adrian Sanchez Cano
Technical Support Engineer
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,257 次查看
motisonnenfeld
Contributor I

Thanks Adrian!

I must have missed that table somehow... :smileyhappy:

Moti

0 项奖励
回复