Kinetis Bootloader for KL05Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Bootloader for KL05Z

3,078 次查看
austinbuchan
Contributor I

I'm interested in porting the Kinetis Bootloader to the KL05Z family of microcontrollers. My goal would be able to bootload an MKL05Z32 over I2C using the KBOOT application (I'm using a FRDM-KL05Z board for development now). I've successfully modified, compiled in IAR, programmed, and run the bootloader for a KL25Z board, but porting to the KL05Z has not gone smoothly. I've tried following the instructions in chapter 10 of the Kinetis Bootloader Reference Manual, but it looks like the bootloader-compatible device header files do not exist for the KL05Z family. Does anyone have a working port of the bootloader for KL05Z, or can you point me in the right direction for finding or generating the appropriate header files?

4 回复数

2,784 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Austin:

I am checking internally if we have the required header files for the KL05. Let me come back to you as soon as I get some feedback.

Regards!

Jorge Gonzalez

2,784 次查看
davidbiancolin
Contributor I

I too am interested in such files, if they exist. :smileyhappy:

0 项奖励
回复

2,784 次查看
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Austin and David:

Sorry for the delay. I just received the required KL05 files. Please find them in the attached ZIP.

Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,784 次查看
RuiFaria
Contributor III

I'm also interesting in porting Kinetis Bootloader to the KL15 family. Could you send to me the required header files for the KL15?

Thank you in the advance,

Rui Faria

0 项奖励
回复