Kinetis Bootloader Download Antivirus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kinetis Bootloader Download Antivirus

Jump to solution
3,386 Views
ken_sallings1
Contributor III

I am having trouble downloading the Kinetis Bootloader 2.0.0.  My antivirus software picks up Mfgtool2.exe as a virus.  See the attached screenshot.  Is this a legitimate hit or is F-Secure issuing a false positive? 

Tags (1)
0 Kudos
Reply
1 Solution
3,301 Views
ken_sallings1
Contributor III

I had to download the image within a Linux VM.  Then I extracted the zip file and removed the MfgTool2.exe and then I copied the bootloader over to my Win7 machine.  I am using F-Secure antivirus.

All is well now.

Ken

View solution in original post

0 Kudos
Reply
2 Replies
3,301 Views
miduo
NXP Employee
NXP Employee

Hi,

Do not know which antivirus software you are using. Actually I am using Symantec and without any problem to download the bootloader. So for your case, is it OK to disable the antivirus software temporarily till the download finished?

0 Kudos
Reply
3,302 Views
ken_sallings1
Contributor III

I had to download the image within a Linux VM.  Then I extracted the zip file and removed the MfgTool2.exe and then I copied the bootloader over to my Win7 machine.  I am using F-Secure antivirus.

All is well now.

Ken

0 Kudos
Reply