Kinetis Bootloader Download Antivirus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis Bootloader Download Antivirus

ソリューションへジャンプ
3,553件の閲覧回数
ken_sallings1
Contributor III

I am having trouble downloading the Kinetis Bootloader 2.0.0.  My antivirus software picks up Mfgtool2.exe as a virus.  See the attached screenshot.  Is this a legitimate hit or is F-Secure issuing a false positive? 

タグ(1)
0 件の賞賛
返信
1 解決策
3,468件の閲覧回数
ken_sallings1
Contributor III

I had to download the image within a Linux VM.  Then I extracted the zip file and removed the MfgTool2.exe and then I copied the bootloader over to my Win7 machine.  I am using F-Secure antivirus.

All is well now.

Ken

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,468件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Do not know which antivirus software you are using. Actually I am using Symantec and without any problem to download the bootloader. So for your case, is it OK to disable the antivirus software temporarily till the download finished?

0 件の賞賛
返信
3,468件の閲覧回数
ken_sallings1
Contributor III

I had to download the image within a Linux VM.  Then I extracted the zip file and removed the MfgTool2.exe and then I copied the bootloader over to my Win7 machine.  I am using F-Secure antivirus.

All is well now.

Ken

0 件の賞賛
返信