Kinetis Bootloader 1.2 not working with TWR-MKV31F51212

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kinetis Bootloader 1.2 not working with TWR-MKV31F51212

1,624 次查看
stevenneves
Contributor I

I have tested this now with a MK22F51212 Tower and this MKV31.  The K22 worked just fine.  I basically followed the attached Demo App User's Guide using both boards.  The bootloader itself flashes properly to both.  I am able to use blhost.exe with both and use the get-property 1 command and get a valid response from both.  The issue lies with Figure 10, Section 5.7.  I set the image and offset for the two boards (I am sure to use the correct led_demo binary for the proper eval board) and upon pressing update, the K22 erases the flash and writes the led_demo image and works properly while the KV31 can not get past erasing flash and instead I am greeted with "No response packet from target device.". 

0 项奖励
回复
2 回复数

1,445 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Steven,

I was wonder if you can share the version of TWR-KV31F120M and specific product number of the KV31.

And I'd also like to know which line of code stucks in when you debug the tower_bootloader demo from the Kinetis_Bootloader_1_2_0.

I'm looking forward to your reply.
Have a great day,
Ping

2015-11-16_17-22-10.jpg

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,445 次查看
mjbcswitzerland
Specialist V

Steven

There is a KBOOT binary for the TWR-KV31F120M (and an application) at http://www.utasker.com/kinetis/TWR-KV31F120M.html

Check that it works on your board to ensure that you have no HW problem.

Regards

Mark

0 项奖励
回复