Kenitis KL05 DMA channel source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kenitis KL05 DMA channel source

2,101件の閲覧回数
cfk
Contributor I

1.pngHi,i am recently use Kenitis family MCU KL05Z32 , but i conldn't find the dma channel source's details ,neither datasheet nor RM document,where could i find the dma request source of KL05? Could somebody help me?

0 件の賞賛
返信
3 返答(返信)

2,049件の閲覧回数
migry
Contributor I

Having used DMA in a small number of experimental configurations, and found the documentation "lacking".

I think naming this field as "SOURCE" is confusing.

DMA transfers are triggered by some event, which can include a ALWAYS trigger.

The SOURCE is the source of the TRIGGER.

For some reason the PIT timer gets a special feature in that the TRIG selects the PIT timer overflow as the trigger, but with limitations that you can only use DMA0 with PIT0, DMA1 with PIT1, etc.

While some of the trigger "sources" are obvious, there are a few which I couldn't figure out from the reference manual.

0 件の賞賛
返信

2,025件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As the section 3.4.8.1 DMA MUX request sources, the source number in Table  20 define the DMA request source.

The DMA triggering source can only be PITx channel, this is a special case, it can manipulate GPIO with PIT cycle.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信

2,070件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to section 3.4.8.1 DMA MUX Request Sources in reference manual of KL05.

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1704253019366.png

 

0 件の賞賛
返信