KW45 10dbm Tx Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW45 10dbm Tx Configuration

1,738件の閲覧回数
MSM1
Contributor I

Hello,

I have Enabled 10dbm Tx by software :

#define mAdvertisingDefaultTxPower_c 10

#define mConnectionDefaultTxPower_c 10

#define gAppMaxTxPowerDbm_c 10

Is there other required configuration ?

Do i need modification in the hardware board ?

Kind Regards,

MSM.

0 件の賞賛
返信
3 返答(返信)

1,722件の閲覧回数
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

\Thank you for contacting NXP support.

That is all you require and also update the Txs_SetTxPowerLevel, in hardware there is no other requirement.

Did you have any troubles? If so please let me know the following information:

  • What SDK version are you using?
  • If you are using an SDK example, what example are you using?
  • Are you using a custom or EVK board?

Please let me know if there is anything else where I can help you.

0 件の賞賛
返信

1,693件の閲覧回数
MSM1
Contributor I

Hello,

Thanks for the quick answer. I am using KW45-EVK just measuring the consumption.

No functional trouble i think we can close this ticket.

But i have issue with measuring consumption's solution. It is another ticket:

https://community.nxp.com/t5/Kinetis-Microcontrollers/KW45-Power-measurment-board-issue/m-p/1869426#...

Thanks for the help.

Regards.

0 件の賞賛
返信

1,673件の閲覧回数
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

No problem, I'm glad to know that everything is fine with this query.

Regarding the other case my college will continue the support on that specific case, in order to proportionate a solution.

I will close this case then, hope you have a good day.

0 件の賞賛
返信