KW45 10dbm Tx Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW45 10dbm Tx Configuration

1,795 Views
MSM1
Contributor I

Hello,

I have Enabled 10dbm Tx by software :

#define mAdvertisingDefaultTxPower_c 10

#define mConnectionDefaultTxPower_c 10

#define gAppMaxTxPowerDbm_c 10

Is there other required configuration ?

Do i need modification in the hardware board ?

Kind Regards,

MSM.

0 Kudos
Reply
3 Replies

1,779 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

\Thank you for contacting NXP support.

That is all you require and also update the Txs_SetTxPowerLevel, in hardware there is no other requirement.

Did you have any troubles? If so please let me know the following information:

  • What SDK version are you using?
  • If you are using an SDK example, what example are you using?
  • Are you using a custom or EVK board?

Please let me know if there is anything else where I can help you.

0 Kudos
Reply

1,750 Views
MSM1
Contributor I

Hello,

Thanks for the quick answer. I am using KW45-EVK just measuring the consumption.

No functional trouble i think we can close this ticket.

But i have issue with measuring consumption's solution. It is another ticket:

https://community.nxp.com/t5/Kinetis-Microcontrollers/KW45-Power-measurment-board-issue/m-p/1869426#...

Thanks for the help.

Regards.

0 Kudos
Reply

1,730 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

No problem, I'm glad to know that everything is fine with this query.

Regarding the other case my college will continue the support on that specific case, in order to proportionate a solution.

I will close this case then, hope you have a good day.

0 Kudos
Reply