KW41Z demo does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW41Z demo does not work

1,236 Views
andrewforsman
Contributor I

I am attempting to run the KW41Z RGB LED demo that comes loaded on the device out of the box. However, when I plug the KW41Z in via USB, the RGB LEDs only cycles for a second before going out and LED2 being illuminated instead. Any ideas as to what causes the demo to run briefly and then fail?

I am connecting the device to a laptop running Windows 10.

Labels (1)
0 Kudos
Reply
1 Reply

1,177 Views
chris_brown
NXP Employee
NXP Employee

HI andrewforsman‌,

I am a little unclear. Have you just gotten your board and immediately plugged it to find this failure?  Or did the board initially work, and then you programmed a project onto the board to find this failure?  If the second one, can you be a little more specific as to which project you programmed onto the board?  A screenshot from your host computer's file system would be helpful. 

Thanks,

Chris

0 Kudos
Reply