KW38's CS cannot be controlled through gpio.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW38's CS cannot be controlled through gpio.

ソリューションへジャンプ
5,485件の閲覧回数
tedwu1
Contributor III

Hello friend,

I want to use gpio as CS because I have 3 SPI devices. I use frdmkw38_dspi_polling_b2b_transfer_master project. But the CS (PTA19) pin always high. I cannot control it to low. I modified some code as follows. Can anyone guide me? Thank you in advance.

Best wishes

Ted Wu

pin_mux.c
void BOARD_InitPins(void)
{
...
/* PORTA16 (pin 4) is configured as SPI1_SOUT */
PORT_SetPinMux(PORTA, 16U, kPORT_MuxAlt2);

/* PORTA17 (pin 5) is configured as SPI1_SIN */
PORT_SetPinMux(PORTA, 17U, kPORT_MuxAlt2);

/* PORTA18 (pin 6) is configured as SPI1_SCK */
PORT_SetPinMux(PORTA, 18U, kPORT_MuxAlt2);

/* PORTA19 (pin 7) is configured as SPI1_PCS0 */
PORT_SetPinMux(PORTA, 19U, kPORT_MuxAsGpio);

PORTA->PCR[19] = ((PORTA->PCR[19] &
/* Mask bits to zero which are setting */
(~(PORT_PCR_SRE_MASK | PORT_PCR_ISF_MASK)))

/* Slew Rate Enable: Fast slew rate is configured on the corresponding pin, if the pin is
* configured as a digital output. */
| PORT_PCR_SRE(kPORT_FastSlewRate));
....
}


dspi_polling_b2b_transfer_master.c
int main(void)
{
BOARD_InitPins();
BOARD_BootClockRUN();
BOARD_InitDebugConsole();

/* Define the init structure for the output pin */
gpio_pin_config_t gpio_1_config = {
kGPIO_DigitalOutput,
1,
};
...
srcClock_Hz = DSPI_MASTER_CLK_FREQ;
DSPI_MasterInit(EXAMPLE_DSPI_MASTER_BASEADDR, &masterConfig, srcClock_Hz);

/* Init output CS GPIO. */
GPIO_PinInit(GPIOA, 19U, &gpio_1_config);

while (1)
{
...
/* Start master transfer, send data to slave */
masterXfer.txData = masterTxData;
masterXfer.rxData = NULL;
masterXfer.dataSize = TRANSFER_SIZE;
masterXfer.configFlags = kDSPI_MasterCtar0;
GPIO_PinWrite(GPIOA, 1U << 19, 0);
DSPI_MasterTransferBlocking(EXAMPLE_DSPI_MASTER_BASEADDR, &masterXfer);
GPIO_PinWrite(GPIOA, 1U << 19, 1);
...
}

0 件の賞賛
返信
1 解決策
5,451件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Just as a quick test you can try the following:

In pin_mux.c > BOARD_InitPins(), add 

PORT_SetPinMux(PORTC, 3U, kPORT_MuxAsGpio);

In dspi_transfer_master.c, add the following after pins and clock initialization:

gpio_pin_config_t gpio_as_cs = {
kGPIO_DigitalOutput,
1,
};

GPIO_PinInit(GPIOC, 3U, &gpio_as_cs);

After that, try writing the GPIO output:

GPIO_PinWrite(GPIOC, 3U, 0);
/* Delay */
for (i = 0U; i < EXAMPLE_DSPI_DEALY_COUNT; i++)
{
__NOP();
}
GPIO_PinWrite(GPIOC, 3U, 1);

You should see that the GPIO output level changes. However, please consider taking a look at the FRDM-KW38 schematics file to confirm that the pin you are trying to configure is not being used or connected to another module.

Please, let me know your findings.

Regards,
Eduardo.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
5,456件の閲覧回数
tedwu1
Contributor III

Hi @EduardoZamora 

If I use a single SPI, I can control the PTA19 (CS) potential level through the SPI program. But I have 3 SPI devices. I want to use gpio as CS (chip select) to distinguish which SPI is used at a time. So I want to use gpio as CS. But if I use gpio as CS I can't control it.

Best wishes

Ted Wu

0 件の賞賛
返信
5,452件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Just as a quick test you can try the following:

In pin_mux.c > BOARD_InitPins(), add 

PORT_SetPinMux(PORTC, 3U, kPORT_MuxAsGpio);

In dspi_transfer_master.c, add the following after pins and clock initialization:

gpio_pin_config_t gpio_as_cs = {
kGPIO_DigitalOutput,
1,
};

GPIO_PinInit(GPIOC, 3U, &gpio_as_cs);

After that, try writing the GPIO output:

GPIO_PinWrite(GPIOC, 3U, 0);
/* Delay */
for (i = 0U; i < EXAMPLE_DSPI_DEALY_COUNT; i++)
{
__NOP();
}
GPIO_PinWrite(GPIOC, 3U, 1);

You should see that the GPIO output level changes. However, please consider taking a look at the FRDM-KW38 schematics file to confirm that the pin you are trying to configure is not being used or connected to another module.

Please, let me know your findings.

Regards,
Eduardo.

0 件の賞賛
返信
5,431件の閲覧回数
tedwu1
Contributor III

Hi @EduardoZamora 

Thank you very much.

Ted Wu

0 件の賞賛
返信
5,465件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @tedwu1

Hope you are doing well.

According to the FRDM-KW38 schematics (which can be downloaded from the FRDM-KW38 webpage, Design Files section), PTA19 should be connected to FXOS8700CQ Combo Sensor Pin 11 (INT1). Please, consider using another pin as GPIO for your application.

Regards,
Eduardo.

0 件の賞賛
返信