KW36 max supply current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW36 max supply current

ソリューションへジャンプ
3,860件の閲覧回数
jictannu
Contributor III

I would like to know the max current when VDD is 3.3v in KW36, but I could not find it in datasheet. 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,594件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

最大是120mA

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
3,595件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

最大是120mA

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,594件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

May be this will help you.

pastedImage_1.png

pastedImage_2.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,594件の閲覧回数
jictannu
Contributor III

Hi, I think the max supply current is unclear in this table.

0 件の賞賛
返信
3,594件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

The notice 2 has said the analog supply current is the sum of the active or disabled current for each of the analog modules on the device. We should see each module's specification for its supply current.

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,594件の閲覧回数
jictannu
Contributor III

Hi, I sorry for my unclear expression. I would like to know the max current that KW36 can withstand.

0 件の賞賛
返信
3,594件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Hi,

The max current the IO can withstand is 3mA.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
3,594件の閲覧回数
jictannu
Contributor III

你好,我想问的是当KW36的供电电压是3.3v时,KW36能承受的最大的电流是多大

0 件の賞賛
返信