KW36 max supply current

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KW36 max supply current

Jump to solution
3,940 Views
jictannu
Contributor III

I would like to know the max current when VDD is 3.3v in KW36, but I could not find it in datasheet. 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
3,674 Views
nxf56274
NXP Employee
NXP Employee

Hi,

最大是120mA

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
7 Replies
3,675 Views
nxf56274
NXP Employee
NXP Employee

Hi,

最大是120mA

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,674 Views
nxf56274
NXP Employee
NXP Employee

Hi,

May be this will help you.

pastedImage_1.png

pastedImage_2.png

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,674 Views
jictannu
Contributor III

Hi, I think the max supply current is unclear in this table.

0 Kudos
Reply
3,674 Views
nxf56274
NXP Employee
NXP Employee

Hi,

The notice 2 has said the analog supply current is the sum of the active or disabled current for each of the analog modules on the device. We should see each module's specification for its supply current.

 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,674 Views
jictannu
Contributor III

Hi, I sorry for my unclear expression. I would like to know the max current that KW36 can withstand.

0 Kudos
Reply
3,674 Views
nxf56274
NXP Employee
NXP Employee

Hi,

The max current the IO can withstand is 3mA.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
3,674 Views
jictannu
Contributor III

你好,我想问的是当KW36的供电电压是3.3v时,KW36能承受的最大的电流是多大

0 Kudos
Reply