KW36: Sending Wireless uart send uart stream to phone gets error sometimes

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW36: Sending Wireless uart send uart stream to phone gets error sometimes

1,373件の閲覧回数
skalyan2
Contributor IV

Hi,

I am using KW36 W_uart example, KW36 acts as slave, i am trying to send some wireless uart data from KW36 to phone(Samsung A30) , when KW36 trying to send one particular wireless uart data,the below error has come.

What is the issue of the below snapshot, can you please explain the problem and the possible solution ? 

pastedImage_1.png

pastedImage_2.png

Many thanks in advance!


Regards

Sai Kalyana Raman

タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,272件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,


Do you have this behavior with all the mobile phones or is this only happening with that specific model ?

Regards,

Estephania

0 件の賞賛
返信

1,272件の閲覧回数
skalyan2
Contributor IV

Hi Estephania,

I have tested only with two mobiles , Samsung A30 (Android version: 9.0), pixel 3(Android version: 9.0) and it is reproducing in both the phones.

Regards

Sai Kalyana Raman

0 件の賞賛
返信

1,272件の閲覧回数
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

To reproduce it on my side, and to confirm , you are using the IoT Toolbox, the wireless uart examples and which it's the frames that you are having issues with ?

Which it's that particular wireless uart data that it's causing you troubles?

Regards ,
Estephania

0 件の賞賛
返信