KW2x SMAC Documentations

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KW2x SMAC Documentations

2,368件の閲覧回数
isaotakashima
Contributor IV

Our customer would like to make the connectivity test tool using the KW2x SMAC.

They refer the following documents, but they cannot find out the example code and timing chart for the transmit and receive data.

- MKW2xSMACDAUG.pdf

- MKW2xSMACRM.pdf

Please advise as soon as possible.

Best regards,

Takashima

ラベル(1)
タグ(2)
3 返答(返信)

2,016件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

SMAC code is part of the Beekit installation package:

BEEKIT_WIRELESS_CONNECTIVITY_TOOLKIT: BeeKit Wireless Connectivity Toolkit. BeeKit is a stand alone software application that provides a graphical user interface (GUI) in which the user can create, modify, save and update wireless network solutions based on Freescale's protocol...
Format: html Modified: 9/7/2014

Luis

0 件の賞賛
返信

2,016件の閲覧回数
isaotakashima
Contributor IV

Dear Luis,

Thank you for your reply.

I understand that the BeeKit is a stand alone software application that provides a graphical user interface (GUI) in which the user can create.

But the BeeKit Ver3.0.2 does not include Kinetis SMAC codebase.

Currently they don't use the ZigBee and 802.15.4 MAC, bcause they want to reduce code size less than 32KB.

Please advise as soon as possible.

Best regards,

Takashima

0 件の賞賛
返信

2,016件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

No as codebase, check : C:\Program Files\Freescale\SMAC\MKW2x\Demo Apps\Connectivity Test

Luis