KV5x eFlexPWM capture example.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

KV5x eFlexPWM capture example.

跳至解决方案
2,880 次查看
arimendes
Contributor III

Hi,

   I would like to receive an  example showing how to configure the KV5x or KV4x eFlexPWM in capture mode. The example can be at register level or using the KDS 2.x api. And it also can be an example for the MC56F84xxx PWMA/PWMB in capture mode, because the peripheral IP is the same.

 Ari.

1 解答
2,723 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ari,

I have developed an example which can demo the capture function of eFlexPWM module. I post it here.

On the demo code, I generate PWM signals with SM0/SM1/SM2 of PWMA module, I connect the PWMA_0A signal to the PWMA_1X pin so that I can check if the captured value is correct or not.

software configuration:

1)enable all module clock

void CLOCK_init(void)
{
    SIM_PCE3|=0x00FF;  //enable PWMA and PWMB all channels
    SIM_PCE0|=0xFF7F;  //enable all Timer and GPIO A/B/C/D/E/G/F
    SIM_PCE2|=0x180; //enable SAR ADC clock and Cyclic ADC clock
    return;
}

2)I configure the PWMA_1X pin GPIO_G9 as PWMA_1X with the code:

//GPIOG9 PWMB_1X PWMA_1X TA3 XB_OUT11, pin 30 on J503 on TWR-8400 board
//connect the measured signal to PWMA_1A pin GPIOG9, test the duty cycle of the signal
void pinPWMA_1X(void)
{
    //let PWMA_1X signal output
    GPIOG_PER|=0x200;
    SIM_GPSGH&=~(0x30);
    SIM_GPSGH|=0x01<<2; //set G9 bits to be 01 in binary:01 Function = PWMA_1X;

   PWMA_OUTEN&=~(0x0F); //disable all PWMA_X pins
}

configure the GPIO_G9 as PWMA_1X: clear the corresponding bit in PWMA_OUTEN, the PWMA_1X will be a capture signal input, set the orresponding bit in PWMA_OUTEN, the PWMA_1X will be an PWM signal output.

3)configure capture function:

void captureFuncPWMA_1A(void)
{
    //bit setting:
    //EDGCNTX_EN=1 Edge counter enabled
    //INP_SELX=0 Raw PWM_X input signal selected as source.
    //EDGX1=01 Capture falling edges
    //EDGX0=10 Capture rising edges
    //ONESHOTX=0 Free running mode is selected.
    PWMA_SM1CAPTCTRLX&=0x00;
    PWMA_SM1CAPTCTRLX=0x98;
    PWMA_SM1CAPTCTRLX|=0x01; //start capture function
    PWMA_OUTEN&=~(0x0F); //disable all PWMA_X pins
}

4)interrupt mode configuration:

void PWM_ISR_SETTING()
{
    //interrupt priority setting
    INTC_IPR8|=0xC000; //set PWMA_CAP interrupt source priority
    //enable the PWM_SM0 reload interrupt
    PWMA_SM1INTEN|=0x80; //edge1(falling edge) trigger interrupt
    
    return;
    
}

5)ISR function of capture:

#pragma interrupt on
void captureISR(void)
{
    static unsigned int i=0;
    varEdge0[i]=PWMA_SM1CVAL0;
    varEdge1[i]=PWMA_SM1CVAL1;
    varDiff[i]=varEdge1-varEdge0;    
    varsm0cnt[i]=PWMA_SM0CNT;
    varsm1cnt[i]=PWMA_SM1CNT;
    i++;
    if(i>=50)
        {
        asm(debughlt);
        }
    //clear the interrupt flag
    PWMA_SM1STS|=0xC0; //clear the CFX1 and CFX0 bits
    
    asm(nop);
    GPIOA_DR^=0x100; //toggle the A8 bit
}

Hardware connection:

I developed the project on CodeWarrior for mcu ver10.6 and TWR-8400 board. Connect the PWMA_0A(pin 40 of primary A connector) to GPIO_G9(pin 30 of J503), it is okay. you'd better connect a 2~5K ohm serial resistor when you test in case you configure both pin as output by mistake.

BR

Xiangjun Rong

在原帖中查看解决方案

3 回复数
2,723 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ari,

Based on your requirement, I am developing the application of capture function, I will post the code based on TWR-8400 board, pls be patient.

BR

Xiangjun rong

0 项奖励
回复
2,724 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Ari,

I have developed an example which can demo the capture function of eFlexPWM module. I post it here.

On the demo code, I generate PWM signals with SM0/SM1/SM2 of PWMA module, I connect the PWMA_0A signal to the PWMA_1X pin so that I can check if the captured value is correct or not.

software configuration:

1)enable all module clock

void CLOCK_init(void)
{
    SIM_PCE3|=0x00FF;  //enable PWMA and PWMB all channels
    SIM_PCE0|=0xFF7F;  //enable all Timer and GPIO A/B/C/D/E/G/F
    SIM_PCE2|=0x180; //enable SAR ADC clock and Cyclic ADC clock
    return;
}

2)I configure the PWMA_1X pin GPIO_G9 as PWMA_1X with the code:

//GPIOG9 PWMB_1X PWMA_1X TA3 XB_OUT11, pin 30 on J503 on TWR-8400 board
//connect the measured signal to PWMA_1A pin GPIOG9, test the duty cycle of the signal
void pinPWMA_1X(void)
{
    //let PWMA_1X signal output
    GPIOG_PER|=0x200;
    SIM_GPSGH&=~(0x30);
    SIM_GPSGH|=0x01<<2; //set G9 bits to be 01 in binary:01 Function = PWMA_1X;

   PWMA_OUTEN&=~(0x0F); //disable all PWMA_X pins
}

configure the GPIO_G9 as PWMA_1X: clear the corresponding bit in PWMA_OUTEN, the PWMA_1X will be a capture signal input, set the orresponding bit in PWMA_OUTEN, the PWMA_1X will be an PWM signal output.

3)configure capture function:

void captureFuncPWMA_1A(void)
{
    //bit setting:
    //EDGCNTX_EN=1 Edge counter enabled
    //INP_SELX=0 Raw PWM_X input signal selected as source.
    //EDGX1=01 Capture falling edges
    //EDGX0=10 Capture rising edges
    //ONESHOTX=0 Free running mode is selected.
    PWMA_SM1CAPTCTRLX&=0x00;
    PWMA_SM1CAPTCTRLX=0x98;
    PWMA_SM1CAPTCTRLX|=0x01; //start capture function
    PWMA_OUTEN&=~(0x0F); //disable all PWMA_X pins
}

4)interrupt mode configuration:

void PWM_ISR_SETTING()
{
    //interrupt priority setting
    INTC_IPR8|=0xC000; //set PWMA_CAP interrupt source priority
    //enable the PWM_SM0 reload interrupt
    PWMA_SM1INTEN|=0x80; //edge1(falling edge) trigger interrupt
    
    return;
    
}

5)ISR function of capture:

#pragma interrupt on
void captureISR(void)
{
    static unsigned int i=0;
    varEdge0[i]=PWMA_SM1CVAL0;
    varEdge1[i]=PWMA_SM1CVAL1;
    varDiff[i]=varEdge1-varEdge0;    
    varsm0cnt[i]=PWMA_SM0CNT;
    varsm1cnt[i]=PWMA_SM1CNT;
    i++;
    if(i>=50)
        {
        asm(debughlt);
        }
    //clear the interrupt flag
    PWMA_SM1STS|=0xC0; //clear the CFX1 and CFX0 bits
    
    asm(nop);
    GPIOA_DR^=0x100; //toggle the A8 bit
}

Hardware connection:

I developed the project on CodeWarrior for mcu ver10.6 and TWR-8400 board. Connect the PWMA_0A(pin 40 of primary A connector) to GPIO_G9(pin 30 of J503), it is okay. you'd better connect a 2~5K ohm serial resistor when you test in case you configure both pin as output by mistake.

BR

Xiangjun Rong

2,723 次查看
arimendes
Contributor III

Thanks, Xiangjun Rong.

 Ari.

0 项奖励
回复