KV5x Freemaster MCAT Tool Current control id Tuning issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KV5x Freemaster MCAT Tool Current control id Tuning issue

2,672件の閲覧回数
Saransyam
Contributor I

Hi ,


I am using TWR-KV58F220M and TWR-MC-LV3PH Tower System with Linix 45ZWN24-40 Motor.
I Am Facing issue with MCAT tool Tuning of Current Control ID, In MCAT tool as described in user manual i set Id_req :- 1A Iq_req:- 0.1A but in oscilloscope graph is not correct i think it is showing some garbage value. Graph and configuration details are mentioned below. Please also check if there is any issue in configuration parameter. 

Configuration

Saransyam_0-1729748217506.pngSaransyam_0-1729748217506.png

Saransyam_1-1729748266562.pngSaransyam_1-1729748266562.png

Saransyam_2-1729748307446.pngSaransyam_2-1729748307446.png

Saransyam_3-1729748340171.pngSaransyam_3-1729748340171.png

 

 

Graph

Saransyam_4-1729748387016.pngSaransyam_4-1729748387016.png

 

 

0 件の賞賛
返信
1 返信

2,602件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the PMSM motor parameter tuning based on MCAT tools, pls refer to the an4642.pdf, which I attached.

Hope it can help you

BR

XiangJun Rong

0 件の賞賛
返信