ADC Voltage Reference Selection for K32

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC Voltage Reference Selection for K32

Jump to solution
2,251 Views
aberger
Contributor V

I am using the FRDM-K32L2B3 and trying to understand the voltage reference selection for the ADC.  

In the ADC Chapter, the SC2[REFSEL] bits provide the following options:

00Default voltage reference pin pair, that is, external pins VREFH and VREFL
01Alternate reference pair, that is, VALTH and VALTL . This pair may be additional external pins or internal sources depending on the MCU configuration. See the chip configuration information for details specific to this MCU
10Reserved
11

Reserved

 

This seems to conflict with the information from 2.3.3 Analog reference options:

aberger_0-1730502092896.png

How can I select between the 3 options VREFH, 1.2V VREF_OUT, and VDDA?

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,202 Views
Ben_Xu1
NXP Employee
NXP Employee

Hi @aberger,

VREFH pin can be used as filter capacitor pin for high precision 1.2V VREF_OUT. When 1.2V VREF is enabled, VREFH is 1.2V VREF_OUT. Also, when 1.2V VREF module is enabled, adding supply to VREFH pad, which is a dedicated 1.2 VREF_OUT pad, from external is prohibited. 

1. ADC0_SC2[REFSEL] = 00b, VREFV1 module disabled, ADC reference voltage is VREFH.

2. ADC0_SC2[REFSEL] = 00b, VREFV1 module enabled, ADC reference voltage is 1.2V VREF_OUT.

3. ADC0_SC2[REFSEL] = 01b, ADC reference voltage is VDDA.

Thanks & Regards,

Ben

View solution in original post

0 Kudos
Reply
1 Reply
2,203 Views
Ben_Xu1
NXP Employee
NXP Employee

Hi @aberger,

VREFH pin can be used as filter capacitor pin for high precision 1.2V VREF_OUT. When 1.2V VREF is enabled, VREFH is 1.2V VREF_OUT. Also, when 1.2V VREF module is enabled, adding supply to VREFH pad, which is a dedicated 1.2 VREF_OUT pad, from external is prohibited. 

1. ADC0_SC2[REFSEL] = 00b, VREFV1 module disabled, ADC reference voltage is VREFH.

2. ADC0_SC2[REFSEL] = 00b, VREFV1 module enabled, ADC reference voltage is 1.2V VREF_OUT.

3. ADC0_SC2[REFSEL] = 01b, ADC reference voltage is VDDA.

Thanks & Regards,

Ben

0 Kudos
Reply