KV58: what are the jitters on the timers output pins?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KV58: what are the jitters on the timers output pins?

919 次查看
iainristmt
Contributor I

I require several low jitter timer outputs. I want to known which timer output pins will provide the lowest jitter.

Is there a difference in jitter between:

  1. The FlexTimer and eFlexPWM modules?
  2. Individual FlexTimer or eFlexPWM modules?
  3. Individual channels of the FlexTimer and eFlexPWM modules?
标签 (1)
0 项奖励
回复
1 回复

804 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi lain,

There is no jitter data for MCGOUTCLK and MCGFFCLK. If they share same clock source, their jitter is almost same. But I prefer eFlexPWM. Because MCGFFCLK is synchronized to the peripheral bus clock. The circuit may affect MCKFFCLK jitter. If they use different clock source, you may check each clock source's jitter. For example, FLL's jitter is not good.

Regards,

Jing

0 项奖励
回复