KV58: what are the jitters on the timers output pins?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KV58: what are the jitters on the timers output pins?

922件の閲覧回数
iainristmt
Contributor I

I require several low jitter timer outputs. I want to known which timer output pins will provide the lowest jitter.

Is there a difference in jitter between:

  1. The FlexTimer and eFlexPWM modules?
  2. Individual FlexTimer or eFlexPWM modules?
  3. Individual channels of the FlexTimer and eFlexPWM modules?
ラベル(1)
0 件の賞賛
返信
1 返信

807件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi lain,

There is no jitter data for MCGOUTCLK and MCGFFCLK. If they share same clock source, their jitter is almost same. But I prefer eFlexPWM. Because MCGFFCLK is synchronized to the peripheral bus clock. The circuit may affect MCKFFCLK jitter. If they use different clock source, you may check each clock source's jitter. For example, FLL's jitter is not good.

Regards,

Jing

0 件の賞賛
返信