KV58: Acessing ITCM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,444件の閲覧回数
lsrbigfoot
Contributor IV

I plan to create a few data variables in ITCM (RAM Partition 2) to run a few memory tests on a MKV58F1M0VLQ24 MCU. Do I have to configure register(s) to enable ITCM? If yes then which register(s)?

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
2,368件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi lsrbigfoot

  If you want to create a few data variables in ITCM, you just need to define the data in the related ITCM data range:

pastedImage_1.png

  You don't need to configure any other register.

You can try it on your side.

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,369件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi lsrbigfoot

  If you want to create a few data variables in ITCM, you just need to define the data in the related ITCM data range:

pastedImage_1.png

  You don't need to configure any other register.

You can try it on your side.

If you still have questions about it, please kindly let me know.

Best Regards,

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,368件の閲覧回数
lsrbigfoot
Contributor IV

I tried accessing ITCM to do a few memory tests. Memory appears to be working. Thanks!

0 件の賞賛
返信