KV31F ref manual error: bootloader signal names

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KV31F ref manual error: bootloader signal names

1,154 Views
adomaszek
Contributor I

Document Number: KV31P100M120SF7RM rev.4 02/2016

Section 13.1: Kinetis Flashloader Chip-Specific Information

PTC10 and PTC11 are not available for I2C0.

PTD4 through PTD7 similarly not available for SPI0.

I imagine the port is correct and the signals are wrong.

Regards,

Andrew Domaszek

Edit: to clarify, I downloaded this revision today from the KV3x page here: KV3x: Kinetis KV3x-100–120 MHz, Advanced 3ph FOC / Sensorless Motor Control MCUs based on ARM® Corte...

Labels (1)
0 Kudos
Reply
1 Reply

1,065 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Thank you for the info.

The correct Kinetis Flashloader Peripheral Pinmux should be:

pastedImage_1.png

I will report this document issue to Kinetis product team. Thanks again.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply