KM35 external voltage reference

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KM35 external voltage reference

Jump to solution
3,408 Views
NArn
Contributor II

Hello,

What is the maximum voltage of an external voltage reference for MKM35Z512VLQ7? I am considering using a REF7012, which is 1.25 V +- 0.025%, 2ppm/C.

Best regards

Niclas

0 Kudos
Reply
1 Solution
3,355 Views
NArn
Contributor II

So, no reason to spend any more time in this forum? If the NXP staff can only provide information that I should manage to find myself in the published material, what is the point?

View solution in original post

0 Kudos
Reply
4 Replies
3,366 Views
NArn
Contributor II

Please let me repeat my question: What is the maximum voltage of an external voltage reference for MKM35Z512VLQ7?

0 Kudos
Reply
3,359 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @NArn ,

No such data. I think it should be 1.2V.

 

Regards,

Jing

0 Kudos
Reply
3,356 Views
NArn
Contributor II

So, no reason to spend any more time in this forum? If the NXP staff can only provide information that I should manage to find myself in the published material, what is the point?

0 Kudos
Reply
3,387 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi @NArn ,

As the NOTE of Figure 34-1 in RM says, you can use externally supplied VREF. But there is no data shows what if external VREF is 1.25V, not 1.2V. In fact, most of people use internal VREF. It is good enough.

 

Regards,

Jing

0 Kudos
Reply