KM34Z256 Three-Phase Power Meter - voltage sampling

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KM34Z256 Three-Phase Power Meter - voltage sampling

ソリューションへジャンプ
2,184件の閲覧回数
zbigniew_halat
Contributor I

Hi,

I am building power meter from scratch on the TWR-KM34Z75M dev board, basing on document DRM162 ("KM34Z256 Three-Phase Power Meter Reference Design")  and I confused with Nyqusit frequency for voltage path (16-bit SAR ADC) mentioned in the document which is 3.072MHz
pastedImage_3.png

but software provided in the package has sampling set at 3kHz (AFE and SAR ADC seems to have the same sampling freq)

pastedImage_4.png

Does SAR ADC has some kind of modulator to oversampling the signal and this why document mentions 3.072MHz?

0 件の賞賛
返信
1 解決策
2,056件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi zbigniew halat,

 

SAR ADC included in MKE32Z MCU does not have any oversampling module.

 

Regarding your other question, one of the clock sources the Analog Front End can be selected is a 6.144 MHz clock, as the Nyquist Theorem says the sampling rate must be at least 2fmax. That's why we the document mentions 3.072 MHz as the Nyquist frequency.

 

Hope it helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,057件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi zbigniew halat,

 

SAR ADC included in MKE32Z MCU does not have any oversampling module.

 

Regarding your other question, one of the clock sources the Analog Front End can be selected is a 6.144 MHz clock, as the Nyquist Theorem says the sampling rate must be at least 2fmax. That's why we the document mentions 3.072 MHz as the Nyquist frequency.

 

Hope it helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信