KL82 - how to get rid of clock stretching in I2C slave configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL82 - how to get rid of clock stretching in I2C slave configuration

Jump to solution
1,922 Views
christophapel
Contributor I

we are using KL82 to interface to an I2C host.

Our application has to send 80kB of data to host CPU which is I2C master. All data is available in RAM of KL82 before the first read operation is called.

Host CPU can unfortunately only receive data in 8Byte chunks.

When using I2C slave driver of Mbed Os 5.15.5. the function

int write(const char *data, int length);

results in 11ms clock stretch following the transfer.

Without this clock stretching, the limitation of the host would hardly affect throughput.

But adding 11ms to every 8 Bytes causes the throughput to drop to a totally unacceptable level.

Please let us know if there is a way to get rid of that clock stretching, e.g. using other driver or patching it.

thanks and regards,

Christoph

0 Kudos
Reply
1 Solution
1,912 Views
mjbcswitzerland
Specialist V

Hi

Clock stretching takes place when the slave doesn't react to a read or write for a certain time and is not (normally) controlled by the I2C driver (nor the I2C controller).

See at about 7:00 in this video showing clock stretching in operation due to the fact that the Kinetis processor is presently in the process of programming flash and can't respond to the new I2C data: https://www.youtube.com/watch?v=awREsqeCEzQ

In this case the clock stretching is about 9ms long, whereby generally (when not programing flash) there is essentially no noticeable delay.

If you are using an OS it may be that its driver is in polling mode (rather then interrupt driven) and the task polling it is being scheduled periodically (eg. once every 10ms) which would possibly produce such a situation. An interrupt (or DMA) driven I2C driver mode would be preferable in such a case.

Note: The KL82 has the same I2C controller as the KL03 (in video).

Regards

Mark
uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training or product development requirements

uTasker solution for KL82:
- https://www.utasker.com/kinetis/FRDM-KL82Z.html
I2C:
- https://www.utasker.com/docs/uTasker/uTasker_I2C.pdf

 

View solution in original post

1 Reply
1,913 Views
mjbcswitzerland
Specialist V

Hi

Clock stretching takes place when the slave doesn't react to a read or write for a certain time and is not (normally) controlled by the I2C driver (nor the I2C controller).

See at about 7:00 in this video showing clock stretching in operation due to the fact that the Kinetis processor is presently in the process of programming flash and can't respond to the new I2C data: https://www.youtube.com/watch?v=awREsqeCEzQ

In this case the clock stretching is about 9ms long, whereby generally (when not programing flash) there is essentially no noticeable delay.

If you are using an OS it may be that its driver is in polling mode (rather then interrupt driven) and the task polling it is being scheduled periodically (eg. once every 10ms) which would possibly produce such a situation. An interrupt (or DMA) driven I2C driver mode would be preferable in such a case.

Note: The KL82 has the same I2C controller as the KL03 (in video).

Regards

Mark
uTasker project developer for Kinetis and i.MX RT]
Contact me by personal message or on the uTasker web site to discuss professional training or product development requirements

uTasker solution for KL82:
- https://www.utasker.com/kinetis/FRDM-KL82Z.html
I2C:
- https://www.utasker.com/docs/uTasker/uTasker_I2C.pdf