KL82 QSPi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL82 QSPi

2,580件の閲覧回数
gaobiao315
Contributor I

the application code now exceeds 128K(KL82Z128VMC7),How to download the application code into the plug-in flash。

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

2,439件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi jze duan,

   Do you want to put all the code to the QSPI and run from qspi, or just want to put some part of the code to the qspi flash, and still run from the internal flash?

  If you want to run from the qspi, you can refer to this document:

https://www.nxp.com/docs/en/user-guide/MBOOTQSPIUG.pdf 

  If you just want to copy part of the code to the QSPI, you can refer to my attached code.

Wish it helps you!

If you still have question about it, please kindly let me know.
Have a great day,
kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,439件の閲覧回数
gaobiao315
Contributor I

Hi Kerry Zhou,

Use your development board frdm-kl82z for debugging. According to the operations (MCU Bootloader QuadSPI User's Guide.pdf)in chapter 3 on the PDF file you provided, the prompt is as shown as the error.

微信图片_20181015113719.jpg

0 件の賞賛
返信

2,439件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Duan jz,

     configure-memory address is wrong, you are using 0X02000000, BUT you need to use 0X20000000

pastedImage_1.png

Please try it again.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,439件の閲覧回数
gaobiao315
Contributor I

希望大家能帮助解决一下,谢谢了!

0 件の賞賛
返信