KL46Z not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,325件の閲覧回数
Ricky1
Contributor I

When i connect the board to the front USB port (i've tried both) the green LED that indicates that the board is working doesn't turn on.
I've been trying turning it on while pressing the reset button and it works, but the LED blinks 8 times repeteadly and supposedly that indicates error.

Also, the board doesn't show up when connecting, only shows up when connecting it in bootmode (only the bootloader appears).

I used a virtual box with windows 7 and tried to update the boot and it doesn't do anything, the problem still persists.

If someone could help me with this i'd really appreciate it, thanks.

0 件の賞賛
返信
1 解決策
3,286件の閲覧回数
ErichStyger
Specialist I

Hi @Ricky1 

You probably need a real Windows 7 machine to update the P&E bootloader on it, see

https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-fre...

 

I hope this helps,

Erich

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,287件の閲覧回数
ErichStyger
Specialist I

Hi @Ricky1 

You probably need a real Windows 7 machine to update the P&E bootloader on it, see

https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-fre...

 

I hope this helps,

Erich

0 件の賞賛
返信
3,284件の閲覧回数
Ricky1
Contributor I
You mean the board isn't broken?
I'll see what i can do, thanks.
0 件の賞賛
返信
3,281件の閲覧回数
ErichStyger
Specialist I

No, it is not broken, but older bootloaders on such boards get confused by Win8 or later host OS. Details in the mentioned article.

0 件の賞賛
返信
3,242件の閲覧回数
Ricky1
Contributor I

I've been trying many times but when i copy and paste the BOOTUPDATEAPP and then disconnect and connect, it doesn't start blinking.
It keeps doing the same, if i keep the RESET button pressed before connecting the LED will start blinking like before (8 times and then stopping, not at 1Hz), but if i don't press anything before connecting, the LED won't turn on.

0 件の賞賛
返信
3,222件の閲覧回数
ErichStyger
Specialist I

Are you using a Windows 7 machine (native, not VM)?

0 件の賞賛
返信
3,277件の閲覧回数
Ricky1
Contributor I
Alright then, thank you so much.
0 件の賞賛
返信