KL46Z not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL46Z not working

Jump to solution
3,385 Views
Ricky1
Contributor I

When i connect the board to the front USB port (i've tried both) the green LED that indicates that the board is working doesn't turn on.
I've been trying turning it on while pressing the reset button and it works, but the LED blinks 8 times repeteadly and supposedly that indicates error.

Also, the board doesn't show up when connecting, only shows up when connecting it in bootmode (only the bootloader appears).

I used a virtual box with windows 7 and tried to update the boot and it doesn't do anything, the problem still persists.

If someone could help me with this i'd really appreciate it, thanks.

0 Kudos
Reply
1 Solution
3,346 Views
ErichStyger
Specialist I

Hi @Ricky1 

You probably need a real Windows 7 machine to update the P&E bootloader on it, see

https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-fre...

 

I hope this helps,

Erich

View solution in original post

0 Kudos
Reply
6 Replies
3,347 Views
ErichStyger
Specialist I

Hi @Ricky1 

You probably need a real Windows 7 machine to update the P&E bootloader on it, see

https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-fre...

 

I hope this helps,

Erich

0 Kudos
Reply
3,344 Views
Ricky1
Contributor I
You mean the board isn't broken?
I'll see what i can do, thanks.
0 Kudos
Reply
3,341 Views
ErichStyger
Specialist I

No, it is not broken, but older bootloaders on such boards get confused by Win8 or later host OS. Details in the mentioned article.

0 Kudos
Reply
3,302 Views
Ricky1
Contributor I

I've been trying many times but when i copy and paste the BOOTUPDATEAPP and then disconnect and connect, it doesn't start blinking.
It keeps doing the same, if i keep the RESET button pressed before connecting the LED will start blinking like before (8 times and then stopping, not at 1Hz), but if i don't press anything before connecting, the LED won't turn on.

0 Kudos
Reply
3,282 Views
ErichStyger
Specialist I

Are you using a Windows 7 machine (native, not VM)?

0 Kudos
Reply
3,337 Views
Ricky1
Contributor I
Alright then, thank you so much.
0 Kudos
Reply