KL28 LPI2C Driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL28 LPI2C Driver

2,764件の閲覧回数
testbed
Contributor III

Hello,

Is it possible to send an ACK to the slave  using the LPI2C of KL28 ?

I am trying to interface pn532 to KL28.  The below line i use to read the response from the  pn532.

stat = LPI2C_DRV_MasterReceiveDataBlocking(INST_LPI2C1, rxbuffer, 256, true, OSIF_WAIT_FOREVER);

The above statement works.

Instead of reading 256 bytes every-time i would like to read  byte by byte and stop when the read bytes equal to

the length that was received in the response header.

E.g (probed from analyzer) What i would like to do is this - Get length in red and read only those many bytes in black bold

Start, h48 [ h24 | WR ], h00, h00, hFF, h02, hFE, hD4, h02, h2A, h00, Stop [GetFirmwareVersion]
Start, h49 [ h24 | RD ], h01, h00, h00, hFF, h00, hFF NAK, Stop [ACK]

Start, h49 [ h24 | RD ], h01, h00, h00, hFF, h06, hFA, hD5, h03, h32, h01, h06, h07 NAK, Stop [Response]

Instead of reading worst case 256 bytes for every command (from KL28)

Start, h48 [ h24 | WR ], h00, h00, hFF, h02, hFE, hD4, h02, h2A, h00, Stop
Start, h49 [ h24 | RD ], h01, h00, h00, hFF, h00, hFF NAK, Stop
Start, h49 [ h24 | RD ], h01, h00, h00, hFF, h06, hFA, hD5, h03, h32, h01, h06, h07, hE8, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00, h00 NAK, Stop

I do not want to hard code/keep track of the response length of every command as i am going to be using indataexchange where the data length may vary (less than 256B) and reading 256 bytes each time will not be efficient.

I have successfully implemented the same with the IIC peripheral of KW31Z which has ACK bit generation feature. Just wondering if it is possible with LPI2C...

Thanks

ラベル(2)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

2,473件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

KL28's LPI2C module is different with KW31's I2C module. It send ACK automatically in master mode.

Regards,

Jing

0 件の賞賛
返信

2,473件の閲覧回数
testbed
Contributor III

Thanks Jing. Also i guess once you program the MTDR with a receive command and number of bytes you cannot change the receive size until after the stop command. right ? I get a fifo error if i try doing so apparently because the master is busy and the lpi2c requires that a start be sent before writing to the MTDR...

0 件の賞賛
返信

2,473件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

if you want to stop a polling mode transfer, you can call LPI2C_MasterStop(). If you want to terminate a transfer in non-blocking mode, the LPI2C_MasterTransferAbort() API shall be called.

Regards,

Jing

0 件の賞賛
返信