KL27 rom-bootloader too slow!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL27 rom-bootloader too slow!

Jump to solution
3,096 Views
paolocolombo
Contributor III

Hi to all,

I'm using rom-bootloader on KL27Z256 on USB. It works corretly, but I think that it's too slow.

In fact, to program 52Kbyte software takes 3 minutes and 15 seconds!

Communication seems to be OK: USB packets travel at 5MHz, and see a package every 1ms. What's the problem then?

It is correct that it is so slow?

Thanks, to all.!

Paolo Colombo

0 Kudos
Reply
1 Solution
2,755 Views
mjbcswitzerland
Specialist V

Hi Paolo

Regards

Mark

View solution in original post

0 Kudos
Reply
4 Replies
2,755 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Paolo Colombo:

This is a problem with the HID USB bootloader. The new release of KBOOT (v1.2) is estimated to be released this week and the problem will be fixed already.

Regards!

Jorge Gonzalez

0 Kudos
Reply
2,755 Views
paolocolombo
Contributor III

Hi,

It's been two weeks. Is there any new news about KBoot V. 1.2?

You know when it will be released?

0 Kudos
Reply
2,755 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Paolo:

The new version is in the page already: Kinetis Bootloader|Freescale

Regards!

Jorge Gonzalez

0 Kudos
Reply
2,756 Views
mjbcswitzerland
Specialist V

Hi Paolo

Regards

Mark

0 Kudos
Reply