KL27 rom-bootloader too slow!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL27 rom-bootloader too slow!

ソリューションへジャンプ
3,154件の閲覧回数
paolocolombo
Contributor III

Hi to all,

I'm using rom-bootloader on KL27Z256 on USB. It works corretly, but I think that it's too slow.

In fact, to program 52Kbyte software takes 3 minutes and 15 seconds!

Communication seems to be OK: USB packets travel at 5MHz, and see a package every 1ms. What's the problem then?

It is correct that it is so slow?

Thanks, to all.!

Paolo Colombo

ラベル(3)
0 件の賞賛
返信
1 解決策
2,813件の閲覧回数
mjbcswitzerland
Specialist V

Hi Paolo

Regards

Mark

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,813件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Paolo Colombo:

This is a problem with the HID USB bootloader. The new release of KBOOT (v1.2) is estimated to be released this week and the problem will be fixed already.

Regards!

Jorge Gonzalez

0 件の賞賛
返信
2,813件の閲覧回数
paolocolombo
Contributor III

Hi,

It's been two weeks. Is there any new news about KBoot V. 1.2?

You know when it will be released?

0 件の賞賛
返信
2,813件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Paolo:

The new version is in the page already: Kinetis Bootloader|Freescale

Regards!

Jorge Gonzalez

0 件の賞賛
返信
2,814件の閲覧回数
mjbcswitzerland
Specialist V

Hi Paolo

Regards

Mark

0 件の賞賛
返信