KL27 ADC external circuit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL27 ADC external circuit

1,581 Views
jh0
Contributor IV

Hi,

I will use KL27 ADC to measure up to 7V. Device will run on 1.8-3.3V.

I use measuring of up to 3.3V (during software development) with resistor divider (2 resistors, 1k5 to GND, 4k5 to VDD), and everything related to software is OK.

Question is related to external input stage, because didn't found anything except Figure 35. (High voltage measurement with an ADC input) in device datasheet. What can be omitted from this setup, for safety measuring up to 7V?

Regards,

Josip

Labels (1)
1 Reply

1,510 Views
bobpaddock
Senior Contributor III

Take ideas from the OP159.  See the 'Technical Documents' section near the bottom:

INA159 data sheet, product information and support | TI.com