KL16 low power crystal startup time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL16 low power crystal startup time

1,586 Views
chipweller
Contributor II

I am using a MKL16Z256VLH4 with a 32768 Hz crystal running in lower power mode (HGO=0).  The datasheet lists the typical crystal startup time (tsct) as 750 ms, and I do see something like that.

My question is what should I assume for the maximum time. Currently I am using 1 second. The processor is running at 3.0V (+/-4%) and the expected die temperature range is 15C to 45C.

Thanks

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,437 Views
Paul_Tian
NXP Employee
NXP Employee

Hi, Weller

Sorry, we do not provide max. value of startup time. But I think you can use this 1 second value first. Thanks.

Best Regards

Paul

0 Kudos
Reply