KL15 ADC VREF Current

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL15 ADC VREF Current

1,527件の閲覧回数
RussellPead
Contributor II

I want to verify the TI REF3033 does not exceed the current or voltage tolerance specs.

1) For the KL15, what is the ADC VREF current min/max and voltage tolerance?

2) Are there any recommend external voltage references to use for the ADC?

タグ(2)
0 件の賞賛
返信
1 返信

1,216件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

HI,

1> KL15 ADC VREFH voltage could up to 3.6V, same with VDDA voltage level. VREFL is same with VSSA. There is no ADC VREF pins current data.

2> In general, we recommend to use VREFH = VDDA, VREFL = VSSA.

Customer could check below link about how to design KL15 ADC module hardware and software to get more accuracy performance:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4373.pdf


Wish it helps.
best regards
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信