KL03 DAC output pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,917件の閲覧回数
markrages
Contributor I

I'm designing a board with the KL03 which uses the 6-bit DAC.

What pin does the voltage appear on?  I don't want to use the internal comparator.

Regards,

Mark

[email protected]

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,780件の閲覧回数
markrages
Contributor I

From the datasheet:

"The 6-bit DAC from a comparator is available as an on-chip internal signal only and is not available externally to a pin."

Ah well, back to xmega for this project then,

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,781件の閲覧回数
markrages
Contributor I

From the datasheet:

"The 6-bit DAC from a comparator is available as an on-chip internal signal only and is not available externally to a pin."

Ah well, back to xmega for this project then,

0 件の賞賛
返信
1,780件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Mark Rages:

That is correct, the 6-bit DAC in KL03 is only internal. Sorry for this inconvenience.

You could look at the KL05 family, which integrates a 12-bit DAC with output pin.

Regards!

Jorge Gonzalez

0 件の賞賛
返信