KL03 DAC output pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL03 DAC output pin

Jump to solution
1,921 Views
markrages
Contributor I

I'm designing a board with the KL03 which uses the 6-bit DAC.

What pin does the voltage appear on?  I don't want to use the internal comparator.

Regards,

Mark

[email protected]

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,784 Views
markrages
Contributor I

From the datasheet:

"The 6-bit DAC from a comparator is available as an on-chip internal signal only and is not available externally to a pin."

Ah well, back to xmega for this project then,

View solution in original post

0 Kudos
Reply
2 Replies
1,785 Views
markrages
Contributor I

From the datasheet:

"The 6-bit DAC from a comparator is available as an on-chip internal signal only and is not available externally to a pin."

Ah well, back to xmega for this project then,

0 Kudos
Reply
1,784 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Mark Rages:

That is correct, the 6-bit DAC in KL03 is only internal. Sorry for this inconvenience.

You could look at the KL05 family, which integrates a 12-bit DAC with output pin.

Regards!

Jorge Gonzalez

0 Kudos
Reply