KL02 I2C User Manual Error (quite the boner too...!)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KL02 I2C User Manual Error (quite the boner too...!)

1,044 次查看
mjbcswitzerland
Specialist V

Hi Al

This is the description of I2Cx_FLT in the most up to date KL02 User's manual (Rev 3.1):

pastedImage_1.png

which should however be

pastedImage_3.png

Easy to prove - in slave mode:

1. the STARTF is set when a start condition is detected.
2 if one enables STOPIE (or should it be SSIE?) there is also an interrupt generated on the start condition.
3. It is impossible to clear the I2C interrupt flag in the status register without first writing 0x10 to the I2Cx_FLT register to set STARTF back to 0 beforehand.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html
Kinetis KL02/3/5:
- http://www.utasker.com/kinetis/FRDM-KL02Z.html
- http://www.utasker.com/kinetis/FRDM-KL03Z.html
- http://www.utasker.com/kinetis/FRDM-KL05Z.html
I2C:
- http://www.utasker.com/docs/uTasker/uTasker_I2C.pdf
Videos:
- https://youtu.be/qRzbwW4-QQg
- https://youtu.be/iZEMRiDmHzw


Free Open Source solution: https://github.com/uTasker/uTasker-Kinetis
Working project in 15 minutes video: https://youtu.be/K8ScSgpgQ6M

Professional Kinetis support, one-on-one training and complete fast-track project solutions: http://www.utasker.com/support.html

标签 (1)
标记 (3)
0 项奖励
回复
1 回复

900 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Thank you for your report, and sorry for the inconveniences that this may cause you.

See the feedback from internal team:

Have talk with doc team to update it, and modification is on-going, also doc team will take some time to collect other change to generate a new version, thanks a lot!    Aug 29, 2017

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复