KINETIS TRAINING

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KINETIS TRAINING

1,564件の閲覧回数
yadhukrishnanvm
Contributor III

Hello,

I really want to study how to write the code for all the drivers (like I2C,SPI,UART etc) of kinetis boards. Can anyone tell me is there any video,pdf or ppt for this purpose. I am a beginner to embedded system, so if anyone know this kind of document please send it me. Without a that I cannot understand how to write the code and how to configure the boards..so please... 

0 件の賞賛
返信
3 返答(返信)

1,407件の閲覧回数
yadhukrishnanvm
Contributor III

I have tried to load the board specific firmware image of TWR-K65F180M from the SEGGER - The Embedded Experts - Downloads - J-Link / J-Trace 

but the board is not exiting from the bootloader mode.

0 件の賞賛
返信

1,407件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Yadhukrishnan V M,

   1.About the driver

  You can use our KSDK2.0 for twr-k65f180, which can be downloaded from this link:

Welcome to Kinetis Expert | Kinetis Expert 

  Choose build an sdk, then choose the board as twr-k65f180, generate the according KSDK package.

  2. About the JLINK firmware

   Please use my attached Jlink firmware:JLink_OpenSDA_V2_2015-10-13.bin

  1) board enter bootloader mode

    Unplug the cable, then press the reset button, at the same time, plug the cable between PC and your tower board.

   You will find your board is a device named as "BOOTLOADER"

 2) Send JLink_OpenSDA_V2_2015-10-13.bin to BOOTLOADER, and wait it is finished.

 3) unplug the cable and plug it again

    You will find your board is a device named as JLINK, it means your firmware is updated successfully.

Wish it helps you!

If you still have question, please let me know!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,406件の閲覧回数
yadhukrishnanvm
Contributor III

kerryzhou‌ Thank you... :smileyhappy:

0 件の賞賛
返信