KEAZN64 with External Programmer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEAZN64 with External Programmer

1,826件の閲覧回数
curiosul
Contributor III

Hello! I am trying to program an KEAZN64 microcontroller with and external programmer.

My possibilities are:

Because SDA pins form development board are not soldered I want to use PEMicro Debugger.

The way I have connected Debugger to Microcontroller:

connections.png

Blue and orange lights from debugger are both ON. It means that supply connections are fine and microcontroller is powered on.

The problem is that connection between debugger and chip is failing:

pemicro_debugger.png

Any idea? Do you have any directions/docs to point me on? I am not sure if the connection are correct.

PS: Also if you have any documentation on how to use TRK-KA64 embeded SDA i would highly appreciate.

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 返信

1,609件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I find below the CPU type is incorrect.

Please select the correct CPU type and select SWD interface.

pastedImage_1.png

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信