KEAZN64 with External Programmer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEAZN64 with External Programmer

1,832 Views
curiosul
Contributor III

Hello! I am trying to program an KEAZN64 microcontroller with and external programmer.

My possibilities are:

Because SDA pins form development board are not soldered I want to use PEMicro Debugger.

The way I have connected Debugger to Microcontroller:

connections.png

Blue and orange lights from debugger are both ON. It means that supply connections are fine and microcontroller is powered on.

The problem is that connection between debugger and chip is failing:

pemicro_debugger.png

Any idea? Do you have any directions/docs to point me on? I am not sure if the connection are correct.

PS: Also if you have any documentation on how to use TRK-KA64 embeded SDA i would highly appreciate.

0 Kudos
Reply
1 Reply

1,615 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I find below the CPU type is incorrect.

Please select the correct CPU type and select SWD interface.

pastedImage_1.png

Wish it helps.


Have a great day,
Mike

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply