KEA8 erase

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEA8 erase

2,464件の閲覧回数
Cram
Contributor III

HI there,

 

I have been working with KEA8 (TSSOP 16 pins) + CW11 + MultiLink FX.

After debbug I decided to use 

SIM_SOPT =0x00000000;

In order to use alternate PTA4 and PAT0 functions. Now I want to erase some devices but I cannot do it.

Using flash to file option and then erase whole device, using KEAZN8M4.xml flash configuration.

Following errors appears

Error executing task KEAZN8M4. Wrong expression ${ProjDirPath}/Project_Settings/Debugger/init_kinetis.tcl; Could not expand variable ProjDirPath

If I use debug option there is no change to connect to device, is there any workaround?

Best regards,

Marc

0 件の賞賛
返信
3 返答(返信)

2,442件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

2,427件の閲覧回数
Cram
Contributor III

Hi vincent, 

 

We do not have a Jlink from segger available, we mainly use pemicro tools.

I am using multilink universal FX. Is there any workaround? 

 

Best regards,

0 件の賞賛
返信

2,420件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Sorry, not.

 

You can try to put the reset pin to low in order to try to start to debug it, I do not remember if the Multilink FX can provide the power to the board, I believe with this option will be easier. But I only use the Jlink

Regards

0 件の賞賛
返信