KEA8 erase

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

KEA8 erase

1,584 次查看
Cram
Contributor III

HI there,

 

I have been working with KEA8 (TSSOP 16 pins) + CW11 + MultiLink FX.

After debbug I decided to use 

SIM_SOPT =0x00000000;

In order to use alternate PTA4 and PAT0 functions. Now I want to erase some devices but I cannot do it.

Using flash to file option and then erase whole device, using KEAZN8M4.xml flash configuration.

Following errors appears

Error executing task KEAZN8M4. Wrong expression ${ProjDirPath}/Project_Settings/Debugger/init_kinetis.tcl; Could not expand variable ProjDirPath

If I use debug option there is no change to connect to device, is there any workaround?

Best regards,

Marc

0 项奖励
回复
3 回复数

1,562 次查看
vicentegomez
NXP TechSupport
NXP TechSupport
0 项奖励
回复

1,547 次查看
Cram
Contributor III

Hi vincent, 

 

We do not have a Jlink from segger available, we mainly use pemicro tools.

I am using multilink universal FX. Is there any workaround? 

 

Best regards,

0 项奖励
回复

1,540 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Sorry, not.

 

You can try to put the reset pin to low in order to try to start to debug it, I do not remember if the Multilink FX can provide the power to the board, I believe with this option will be easier. But I only use the Jlink

Regards

0 项奖励
回复