KEA128 flashing failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEA128 flashing failed

Jump to solution
2,710 Views
saya
Contributor III

Hi,everyone:

I am using CW 10.6.

I was able to flash my KEA128 without problems, but all the sudden it won't flashing anymore, I got this error when trying:

fl::target -lc "LC for Simple Flash (2)"

fl::target -b 0x1ffff000 0x4000

fl::target -v off -l off

cmdwin::fl::device -d "FTMRE_PFlash128RAM16" -o "32kx32x1" -a 0x0 0x1ffff

cmdwin::fl::image -f "C:\\..\\TRK-KEA128_Lab1.elf" -t "Auto Detect" -re on -r 0x0 0x1ffff -oe off

cmdwin::fl::erase image

Beginning Operation ...  

-------------------------

Auto-detection is successful. 

  File is of type Elf Format. 

Performing target initialization ...  

Device FTMRE_PFlash128RAM16 is protected 

Erasing ...........

Erase Command Succeeded. 

Device FTMRE_PFlash128RAM16 is protected 

cmdwin::fl::write

-------------------------

Flash Operation.  ...

Auto-detection is successful. 

  File is of type Elf Format. 

Device FTMRE_PFlash128RAM16 is protected 

Programming ....

Device FTMRE_PFlash128RAM16 is protected 

Error:  Program Command Failed.

Error: Program Command Failed.

This happens to any project I am trying to flash into the board.

Any help is appreciated!

Alan

0 Kudos
Reply
1 Solution
2,466 Views
saya
Contributor III

Untitled.png

I figured it out, the initialization and  memory tab were not configured correctly.

View solution in original post

0 Kudos
Reply
2 Replies
2,466 Views
saya
Contributor III

Untitled.png

I changed the connection option, and it is working again, could someone explain this a bit?

0 Kudos
Reply
2,467 Views
saya
Contributor III

Untitled.png

I figured it out, the initialization and  memory tab were not configured correctly.

0 Kudos
Reply