KEA128 MSCAN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEA128 MSCAN

1,671件の閲覧回数
sharadmehta
Contributor I

Need Keil example code/project to read and write CAN Messages.

Board TRK-KEA128

ラベル(1)
0 件の賞賛
返信
1 返信

1,452件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hello,

Hi Sharad Mehta,

   This is the same question as your another post:

KEA128 MSCAN 

  Please check that post, I have answered you.

  You can use the CW project, or you create the KEIL KEA project, then add the CW CAN driver to your keil project, it also works.

  After you create the keil project, and add the MSCAN driver have problems, please let me know.


Have a great day,
kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信