KEA128: Is possible to use the KBI lines as External Interrupts ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KEA128: Is possible to use the KBI lines as External Interrupts ?

1,322件の閲覧回数
cant
Contributor II

KEA128: Is possible to use the KBI lines as External Interrupts ?

Thanks

0 件の賞賛
返信
2 返答(返信)

1,317件の閲覧回数
cant
Contributor II
0 件の賞賛
返信

1,307件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @cant,

Could you please try to enter the website one more time if needed? We have clicked on it and accessed the website without any issue. If you still do not have access, could you please try accessing the website here?

Now, about your original question:

KEA128: Is possible to use the KBI lines as External Interrupts ?

In the KEA128 Sub-Family Reference Manual. Section 35.5 Functional Description., it is mentioned that the KBI could be use as External Interrupts as follows: "[…]these inputs are also useful as extra external interrupt inputs and as an external means of waking the MCU from stop or wait low-power modes."

You might find useful to see the following community post, as there is an implementation of the KBI pins as external interrupts for another Kinetis part: External interrupts on KBI pins of MKE04Z - NXP Community.

Warm regards, Raul.

0 件の賞賛
返信